About IPU preview performance in i.MX6DQ.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About IPU preview performance in i.MX6DQ.

420 Views
keitanagashima
Senior Contributor I

Dear All,

I'd like to know the preview performance in i.MX6DQ.

In the case of input 1080p@60fps video data from MIPI-CSI2, is it possible to use the preview function?

<Q1>

[Data] : 1920(W) * 1080(H) * 60(fps) * 1.35(Blanking) * 24(bit) = 3,844 Mbit/s = 480 MByte/s

[MIPI-CSI2] : 800Mbps/lane for four data lanes configuration = 400 MBytes/s

--> [Data] > [MIPI-CSI2]

From the above results, I consider i.MX6DQ (MIPI-CSI2 I/F) cannot support 1080p@60fps.

Is my understanding correct?

<Q2>

[Data] : 1920(W) * 1080(H) * 60(fps) * 1.35(Blanking) * 16(bit) = 2,563 Mbit/s = 320 MByte/s

-->  [Data] < [MIPI-CSI2]

In this case, is it possible to use the preview function?

I worried about CPU load, data transfer internal IPU, and CSI performance(CSI2IPU gasket: MIPI to CSI),etc.

Please give me advice.

Best Regards,
Keita

Labels (3)
0 Kudos
Reply
1 Reply

350 Views
igorpadykov
NXP Employee
NXP Employee

Hi Keita

1. yes understanding is correct

2.  yes it is possible

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply