Dear All,
Hello. I have a question about double buffer of IPU in i.MX6DQ.
My customer's system will display with double buffer mode in Non-OS program.
And, they tested the display with double buffer mode after the initialization of IPU.
[Result]
Use the Buffer0 earlier : Success
Uses the Buffer1 earlier : Looks flickering
[Question]
When one enable the Double Buffer in IPUx_CH_DB_MODE_SEL0,
Is there limitation on the 1st display?
Ex) First time, it is necessary to use from the side of Buffer0.
Best Regards,
Keita