Dear Sir or Madam,
Hello.
Refer to Figure 18-8. Serial clock generation (Page.828) in MCIMX6DQRM(Rev.2).
I couldn't find the clock source of "ipp_di0_clk" & "ipp_di1_clk".
Is it external clock? And, please tell me the PAD which input the clock for IPU.
Best Regards,
Keita
Solved! Go to Solution.
Hi Keita
according to internal CQ (CT 44041259) design showed the following information:
for the ipp_di0_clk:
Alt2 of pin EIM_DA14 weim.WEIM_DA_A[14] ipu1.DI1_D1_CS ccm.DI0_EXT_CLK
for the ipp_di1_clk:
ALT2 of Pin EIM_DA13 weim.WEIM_DA_A[13] ipu1.DI1_D0_CS ccm.DI1_EXT_CLK
or
ALT2 of Pin EIM_EB2 weim.WEIM_EB[2] ecspi1.SS0 ccm.DI1_EXT_CLK
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Keita
according to internal CQ (CT 44041259) design showed the following information:
for the ipp_di0_clk:
Alt2 of pin EIM_DA14 weim.WEIM_DA_A[14] ipu1.DI1_D1_CS ccm.DI0_EXT_CLK
for the ipp_di1_clk:
ALT2 of Pin EIM_DA13 weim.WEIM_DA_A[13] ipu1.DI1_D0_CS ccm.DI1_EXT_CLK
or
ALT2 of Pin EIM_EB2 weim.WEIM_EB[2] ecspi1.SS0 ccm.DI1_EXT_CLK
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
Thank you for your reply.
i.e. "ipp_di0_clk" & "ipp_di1_clk" are able to select and use as external clock from above PADs, aren't it?
(Is previous your answer mistake? It has already removed.)
Best Regards,
Keita
Hi Keita
yes "ipp_di0_clk" & "ipp_di1_clk" are able to select and use as external clock from above PADs,
I rechecked internal community where found last answer.
Best regards
igor
Hi Igor,
Thank you for your prompt checking.
I couldn't find these description in reference manual.
Will you have plan to describe these IOMUX setting?
Best Regards,
Keita
Hi Keita
I can give you link to that internal community
(please create service request for that), on that link
there was description that this will be added to RM.
Sorry, I can not give date.
Best regards
igor
Hi Igor,
>I can give you link to that internal community
Thank you very much!
>Sorry, I can not give date.
OK. No problem.
Best Regards,
Keita