About IPU clock source in i.MX6DQ.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About IPU clock source in i.MX6DQ.

跳至解决方案
2,390 次查看
keitanagashima
Senior Contributor I

Dear Sir or Madam,

Hello.

Refer to Figure 18-8. Serial clock generation (Page.828) in MCIMX6DQRM(Rev.2).

I couldn't find the clock source of "ipp_di0_clk" & "ipp_di1_clk".

Is it external clock? And, please tell me the PAD which input the clock for IPU.

Best Regards,

Keita

标签 (5)
0 项奖励
回复
1 解答
2,059 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Keita

according to internal CQ (CT 44041259) design showed the following information:

for the ipp_di0_clk:
Alt2 of pin EIM_DA14 weim.WEIM_DA_A[14] ipu1.DI1_D1_CS ccm.DI0_EXT_CLK

for the ipp_di1_clk:
ALT2 of Pin EIM_DA13 weim.WEIM_DA_A[13] ipu1.DI1_D0_CS ccm.DI1_EXT_CLK
or
ALT2 of Pin EIM_EB2 weim.WEIM_EB[2] ecspi1.SS0 ccm.DI1_EXT_CLK


Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
6 回复数
2,060 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Keita

according to internal CQ (CT 44041259) design showed the following information:

for the ipp_di0_clk:
Alt2 of pin EIM_DA14 weim.WEIM_DA_A[14] ipu1.DI1_D1_CS ccm.DI0_EXT_CLK

for the ipp_di1_clk:
ALT2 of Pin EIM_DA13 weim.WEIM_DA_A[13] ipu1.DI1_D0_CS ccm.DI1_EXT_CLK
or
ALT2 of Pin EIM_EB2 weim.WEIM_EB[2] ecspi1.SS0 ccm.DI1_EXT_CLK


Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
2,059 次查看
keitanagashima
Senior Contributor I

Hi Igor,

Thank you for your reply.

i.e. "ipp_di0_clk" & "ipp_di1_clk" are able to select and use as external clock from above PADs, aren't it?

(Is previous your answer mistake? It has already removed.)

Best Regards,

Keita

0 项奖励
回复
2,059 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Keita

yes "ipp_di0_clk" & "ipp_di1_clk" are able to select and use as external clock from above PADs,

I rechecked internal community where found last answer.


Best regards

igor


2,059 次查看
keitanagashima
Senior Contributor I

Hi Igor,

Thank you for your prompt checking.

I couldn't find these description in reference manual.

Will you have plan to describe these IOMUX setting?

Best Regards,

Keita

0 项奖励
回复
2,059 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Keita

I can give you link to that internal community

(please create service request for that), on that link

there was description that this will be added to RM.

Sorry, I can not give date.


Best regards

igor

0 项奖励
回复
2,059 次查看
keitanagashima
Senior Contributor I

Hi Igor,

>I can give you link to that internal community

Thank you very much!

>Sorry, I can not give date.

OK. No problem.


Best Regards,

Keita


0 项奖励
回复