About IOMUX of i.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About IOMUX of i.MX6

Jump to solution
3,185 Views
宗標廖
Contributor V

Hello Community

About pin config of i.mx6, I have two questions.

Q1:

Only pad that used for input can have pull-up resistor, pad that used for output cannot have pull-up resister.

Is it right? why?

Q2:

For Pad Control Register(e.g. IOMUXC_SW_PAD_CTL_PAD_CSI0_DATA18),what does Keeper Enabled mean?

What is Keeper?

pullup.PNG

Best Regards,

ZongbiaoLiao

Labels (1)
1 Solution
2,495 Views
Yuri
NXP Employee
NXP Employee

Hello,

the following app note helps to setup pin’s electrical properties.

“Influence of Pin Setting on System Function and Performance”

http://www.nxp.com/files/32bit/doc/app_note/AN5078.pdf

Regards,

Yuri.

View solution in original post

5 Replies
2,496 Views
Yuri
NXP Employee
NXP Employee

Hello,

the following app note helps to setup pin’s electrical properties.

“Influence of Pin Setting on System Function and Performance”

http://www.nxp.com/files/32bit/doc/app_note/AN5078.pdf

Regards,

Yuri.

2,495 Views
宗標廖
Contributor V

Yuri

Thank you!

0 Kudos
Reply
2,495 Views
igorpadykov
NXP Employee
NXP Employee

Hi ZongbiaoLiao

1. output also can be configured with pull-up resister

2. keeper functionality is explained on

Bus-holder - Wikipedia, the free encyclopedia

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

2,495 Views
宗標廖
Contributor V

Hi Igor

Thank you for you reply.

So there is no relationship between pull-up and the direction of pad.Right?

Best Regards,

ZongbiaoLiao

0 Kudos
Reply
2,495 Views
igorpadykov
NXP Employee
NXP Employee

yes right

Best regards

igor

0 Kudos
Reply