About IOMUX of i.MX6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About IOMUX of i.MX6

跳至解决方案
3,395 次查看
宗標廖
Contributor V

Hello Community

About pin config of i.mx6, I have two questions.

Q1:

Only pad that used for input can have pull-up resistor, pad that used for output cannot have pull-up resister.

Is it right? why?

Q2:

For Pad Control Register(e.g. IOMUXC_SW_PAD_CTL_PAD_CSI0_DATA18),what does Keeper Enabled mean?

What is Keeper?

pullup.PNG

Best Regards,

ZongbiaoLiao

标签 (1)
1 解答
2,705 次查看
Yuri
NXP Employee
NXP Employee

Hello,

the following app note helps to setup pin’s electrical properties.

“Influence of Pin Setting on System Function and Performance”

http://www.nxp.com/files/32bit/doc/app_note/AN5078.pdf

Regards,

Yuri.

在原帖中查看解决方案

5 回复数
2,706 次查看
Yuri
NXP Employee
NXP Employee

Hello,

the following app note helps to setup pin’s electrical properties.

“Influence of Pin Setting on System Function and Performance”

http://www.nxp.com/files/32bit/doc/app_note/AN5078.pdf

Regards,

Yuri.

2,705 次查看
宗標廖
Contributor V

Yuri

Thank you!

0 项奖励
回复
2,705 次查看
igorpadykov
NXP Employee
NXP Employee

Hi ZongbiaoLiao

1. output also can be configured with pull-up resister

2. keeper functionality is explained on

Bus-holder - Wikipedia, the free encyclopedia

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

2,705 次查看
宗標廖
Contributor V

Hi Igor

Thank you for you reply.

So there is no relationship between pull-up and the direction of pad.Right?

Best Regards,

ZongbiaoLiao

0 项奖励
回复
2,705 次查看
igorpadykov
NXP Employee
NXP Employee

yes right

Best regards

igor

0 项奖励
回复