About IOMUX SION bit of last GA version.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About IOMUX SION bit of last GA version.

812 Views
takashitakahash
Contributor III

I confirmed last GA version ,The USDHCx_CMD is Enable with LTIB ,but Yocto has become Disable .

Which one is correct?

Labels (1)
0 Kudos
5 Replies

576 Views
igorpadykov
NXP Employee
NXP Employee

Hi takashi

SION is set by iROM, so yocto may not set it twice.

How did you find that SION is disabled, could you

say procedure ? Had you read iomux register ?

Also had you included uSDHC driver in linux build ?

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos

576 Views
takashitakahash
Contributor III


Hi chip

Do not verify that SION is disable.

There was a terminal which is set bit of SION explicitly pinctrl setting of "imx6qdl.dtsi",

So I think other terminals is SION = disable.

Thanks,

Best Regards.

Takashi Takahashi

0 Kudos

576 Views
igorpadykov
NXP Employee
NXP Employee

Hi takashi

correct SION is enabled.

Best regards

chip

576 Views
takashitakahash
Contributor III


Hi chip

Thankyou for your replay.

Do not hit the Enable explicitly in "imx6qdl.dtsi", etc..

As to Enable, do I need to modify the BSP?

Or consideration  is not required in particular?

Thank you,

Best Regards.

T.Takahashi

0 Kudos

576 Views
igorpadykov
NXP Employee
NXP Employee

Hi takashi

yes I think you can explicitly enable

SION bit in BSP (modify the BSP).

Best regards

chip

0 Kudos