About IMX8MQ uboot display LOGO

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About IMX8MQ uboot display LOGO

3,545件の閲覧回数
Joe_C
Contributor I

I have initialized the MIPI DSI controller, and I can see the clock, data and other waveforms through the oscilloscope, but the logo still cannot be displayed, what should I do?Through debugging, I found that the program called the Splash Screen part of the code, instead of LCD_LOGO.

code1.png

0 件の賞賛
返信
5 返答(返信)

3,540件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi

 

Did you set panel in uboot? As the screenshot shown, default planel is Hannstar-XGA.

setenv panel xxx

 

BR

Zhiming

0 件の賞賛
返信

3,530件の閲覧回数
Joe_C
Contributor I

My question is that Mipi Lane can measure the waveform, but there is no data. What should I do next?

0 件の賞賛
返信

3,522件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Which bsp and soc you are using?

0 件の賞賛
返信

3,506件の閲覧回数
Joe_C
Contributor I

soc:imx8mq

version:4.19.35

タグ(1)
0 件の賞賛
返信

3,244件の閲覧回数
myy
Contributor II

Hi

How do you inited mipi dsi controller? can you give me some help?

0 件の賞賛
返信