About IMX6Q kernel 3.10.53 rotate screen issue.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About IMX6Q kernel 3.10.53 rotate screen issue.

1,783 Views
lifusong
Contributor IV

echo 1 > sys/class/graphics/fb0/rotate ,will rotate 180 degrees.

and see the define in ipu.h

IPU_ROTATE_NONE = 0,
IPU_ROTATE_VERT_FLIP = 1,
IPU_ROTATE_HORIZ_FLIP = 2,
IPU_ROTATE_180 = 3,
IPU_ROTATE_90_RIGHT = 4,
IPU_ROTATE_90_RIGHT_VFLIP = 5,
IPU_ROTATE_90_RIGHT_HFLIP = 6,
IPU_ROTATE_90_LEFT = 7,

write any value of 2 to 7 can't rotate the screen.

how to rotate 90 degrees for fb0.

board imx6q  kernel 3.10.53 

android is linux-2.6-imx.git - Freescale i.MX Linux Tree 

the screen size is 1024*600

and try to rotate the kernel logo with boot args fbcon=rotate:3  will case kernel reset and can't get any debug message.

Labels (3)
Tags (1)
0 Kudos
Reply
1 Reply

1,178 Views
joanxie
NXP TechSupport
NXP TechSupport
0 Kudos
Reply