About IMX6Q-SDB LVDS proting issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About IMX6Q-SDB LVDS proting issue

Jump to solution
1,013 Views
tab_song
Contributor II

QQ图片20170113183149.jpg

我只修改了imx6qdl-sabresd.dtsi里的LVDS1的timing参数,并且依照I.MX_BSP_Poring_Guide.pdf

并添加了uboot启动参数: video=mxcfb0:dev=ldb,if=RGB666

启动就会出现这种情况,半边正常半边花屏,网上有说改ldb.c里的ldb_modedb,但是我在drivers/video/fbdev/mxc/ldb.c里找不到该结构体。

内核版本:4.1.15_2.0.0_ga

i only change the parameter of lvds1`s timing on imx6qdl-sabresd.dtsi,and modify the u-boot parameters according to the I.MX_BSP_Porting_Guide.pdf document.

but as you see,my panal can`t work well.

kernel:4.1.15_2.0.0_ga.

What am I to do?

0 Kudos
Reply
1 Solution
883 Views
tab_song
Contributor II

it`s my mistake, i forget control one pin that select RGB24 or RGB666.

View solution in original post

0 Kudos
Reply
2 Replies
884 Views
tab_song
Contributor II

it`s my mistake, i forget control one pin that select RGB24 or RGB666.

0 Kudos
Reply
883 Views
igorpadykov
NXP Employee
NXP Employee

Hi tab

had you changed kernel boot parameter as in examples in

Table 10. Common kernel boot parameters attached Release Notes.

Also may be useful to check links with examples of bring-up of new lvds lcds

https://community.freescale.com/thread/355690

https://community.freescale.com/thread/373763

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply