About I/O direction of LVDS signals in i.MX6DQ.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About I/O direction of LVDS signals in i.MX6DQ.

Jump to solution
866 Views
keitanagashima
Senior Contributor I

Dear All,

Hello.

I have a question about I/O direction of LVDS signals in i.MX6DQ.

Refer to Table 100. 21 x 21 mm Functional Contact Assignments in IMX6DQAEC(Rev.4).

The direction of LVDS signals was all input.

And, I couldn't find the register of direction setting in Reference Manual.

I consider that LVDS signals only use as output.

[Question]

Where does it change the direction from input to output in U-boot?

Best Regards,

Keita

Labels (6)
0 Kudos
1 Solution
713 Views
igorpadykov
NXP Employee
NXP Employee

Hi Keita

you are right, in i.MX6 LDB LVDS signals only used as output,

setting register LDB_CTRL, field ch0,1_mode[1:0] to "channel enabled"

will enable to output data signal.

Best regards

igor

View solution in original post

0 Kudos
7 Replies
714 Views
igorpadykov
NXP Employee
NXP Employee

Hi Keita

you are right, in i.MX6 LDB LVDS signals only used as output,

setting register LDB_CTRL, field ch0,1_mode[1:0] to "channel enabled"

will enable to output data signal.

Best regards

igor

0 Kudos
713 Views
keitanagashima
Senior Contributor I

Dear Igor,

Sorry. I have an additional question.

During reset period, is the direction of LVDS signals the output?

Best Regards,

Keita

0 Kudos
713 Views
igorpadykov
NXP Employee
NXP Employee

Hi Keita

yes, during reset period the direction of LVDS signals is also output.

Best regards

igor

713 Views
art
NXP Employee
NXP Employee

This is just a typo in the table, all of the LVDS signals are analog differential pairs type.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
713 Views
keitanagashima
Senior Contributor I

Hi Artur,

Thank you for your reply.

Let me clarify my understanding.

- All LVDS signals are always output.

- "Keeper" is typo. And, no pull-up,down.

Is it OK?

Best Regards,

Keita

0 Kudos
713 Views
art
NXP Employee
NXP Employee

Yes, you are right.

Best Regards,

Artur

0 Kudos
713 Views
keitanagashima
Senior Contributor I

Hi Artur,

Thank you very much!

I hope the Data sheet and Reference manual fix the typo in the next update.

DS: Table 100. 21 x 21 mm Functional Contact Assignments in IMX6DQAEC(Rev.4).

RM: Table 39-3. LDB External Signals in IMX6DQRM(Rev.3).

Best Regards,

Keita