About Hot Plug function of PCIe for i.MX8

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About Hot Plug function of PCIe for i.MX8

Jump to solution
2,821 Views
heecheol_jung
Contributor II

As far as I know PCIe hotplug function is supported after linux kernel 4.X.

but i.MX6 isn't support cause chipset limitation
Does i.MX8 support PCIe hotplug in hw?

0 Kudos
Reply
1 Solution
2,575 Views
igorpadykov
NXP Employee
NXP Employee

Hi heecheol

unfortunately PCIe hotplug is not supported by hardware.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

5 Replies
2,576 Views
igorpadykov
NXP Employee
NXP Employee

Hi heecheol

unfortunately PCIe hotplug is not supported by hardware.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,126 Views
kergoth
Contributor I

Is PCIe hotplug still unsupported with the i.MX8 qxpmek rev D boards? I'm assuming this is the case, but looking to confirm.

0 Kudos
Reply
2,114 Views
Yuri
NXP Employee
NXP Employee

@kergoth 
Hello,

     PCIe hotplug still is not supported

Regards,
Yuri.

0 Kudos
Reply
2,106 Views
noorahsan
Contributor II

Hello Yuri,

 

You mean "PCIe hotplug still is not supported"?

 

Regards

2,087 Views
Yuri
NXP Employee
NXP Employee

@noorahsan 

 Correct - still is not supported

~Yuri.

0 Kudos
Reply