About Hot Plug function of PCIe for i.MX8

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About Hot Plug function of PCIe for i.MX8

ソリューションへジャンプ
2,805件の閲覧回数
heecheol_jung
Contributor II

As far as I know PCIe hotplug function is supported after linux kernel 4.X.

but i.MX6 isn't support cause chipset limitation
Does i.MX8 support PCIe hotplug in hw?

0 件の賞賛
返信
1 解決策
2,559件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi heecheol

unfortunately PCIe hotplug is not supported by hardware.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

5 返答(返信)
2,560件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi heecheol

unfortunately PCIe hotplug is not supported by hardware.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,110件の閲覧回数
kergoth
Contributor I

Is PCIe hotplug still unsupported with the i.MX8 qxpmek rev D boards? I'm assuming this is the case, but looking to confirm.

0 件の賞賛
返信
2,098件の閲覧回数
Yuri
NXP Employee
NXP Employee

@kergoth 
Hello,

     PCIe hotplug still is not supported

Regards,
Yuri.

0 件の賞賛
返信
2,090件の閲覧回数
noorahsan
Contributor II

Hello Yuri,

 

You mean "PCIe hotplug still is not supported"?

 

Regards

2,071件の閲覧回数
Yuri
NXP Employee
NXP Employee

@noorahsan 

 Correct - still is not supported

~Yuri.

0 件の賞賛
返信