About HDMI brightness between android 8.1 and android 9

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About HDMI brightness between android 8.1 and android 9

1,076件の閲覧回数
hsuryan
Contributor I

C7EDE296-0DE1-4838-8815-09BB9BEB0C66.jpg

We are facing a problem for the Android 8.1 of display brightness.

We use the same hardware and install the Android 8.1 and Android 9.

The Android 9 shows in the left screen while the Android 8.1 shows in the left one.

The brightness is very different between the two OS version.

We are just wondering how we can adjust the display brightness for Android 8.1 since it's really dark compare to Android 9 base on the same hardware.#

ラベル(2)
0 件の賞賛
返信
1 返信

996件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello,

Can you please try with the below adb command and see if that solves the problem.

adb shell settings put system screen_brightness 255

Hope this can help you.

Best regards,

Diego.

0 件の賞賛
返信