Dear all,
We want to use LPSR mode of i.MX7S.
And we want to wake-up a system by an interrupt from GPIO.
The following is explained in a reference manual.
GPIO1_IO00-IO07 are supplied power to by NVCC_GPIO1, and GPIO1_IO08-IO15 are supplied power to by NVCC_GPIO2.
GPIO1_IO00-IO07 are explained in LPSR.
- 8.2.5 IOMUXC LPSR Memory Map/Register Definition
However, GPIO1_IO8-IO15 are explained in the following(not LPSR).
- 8.2.7 IOMUXC Memory Map/Register Definition
It seems that those are not included in LPSR,
Can GPIO1_IO8-IO15 be used as a wake-up source from LPSR mode?
May I have advice?
Best Regards,
Yuuki
解決済! 解決策の投稿を見る。
Hi Yuuki
>Is GPIO1_IO00-IO07 a mistake of GPIO1_IO08-IO15?
no. It shows just more capabilities for GPIO1_IO00-IO07,
both can be used in LPSR and both wake.
Best regards
igor
Hi Yuuki
>Can GPIO1_IO8-IO15 be used as a wake-up source from LPSR mode?
yes. GPIO1_IO00-IO07 are explained in LPSR since it may have alternative
iomux settings in LPSR.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Dear Igor-san,
Thank you for your support.
> yes. GPIO1_IO00-IO07 are explained in LPSR since it may have alternative iomux settings in LPSR.
=>
Is GPIO1_IO00-IO07 a mistake of GPIO1_IO08-IO15?
Best Regards,
Yuuki
Hi Yuuki
>Is GPIO1_IO00-IO07 a mistake of GPIO1_IO08-IO15?
no. It shows just more capabilities for GPIO1_IO00-IO07,
both can be used in LPSR and both wake.
Best regards
igor
Dear Igor-san,
We checked about these GPIOs in LPSR mode.
NVCC_GPIO1 and NVCC_GPIO2 are supplied power to by VDD_LPSR(1.8V).
In LPSR mode,
GPIO1_IO00-GPIO1_IO07 can hold output High.
However, GPIO1_IO08-GPIO1_IO15 can not hold output High.(The output voltage drops to Low.)
Is there any necessary setting?
GPIO1_IO08-GPIO1_IO15 can be worked normally in LPSR mode?
When it is in RUN mode, GPIO1_IO08-GPIO1_IO15 works normally.
And I understand that GPIO1_IO08-GPIO1_IO15 can be used as wake-up source.
May I have advice?
Best Regards,
Yuuki
Hi Yuuki
>And I understand that GPIO1_IO08-GPIO1_IO15 can be used as wake-up source.
yes they can be used. Note, it should be configured as inputs, not outputs.
Best regards
igor