About ESAI slave connection in i.MX6DQ.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About ESAI slave connection in i.MX6DQ.

Jump to solution
1,894 Views
keitanagashima
Senior Contributor I

Dear All,

Hello.

I have a question about ESAI slave connection in i.MX6DQ.

Refer to attached file and please check the clock connection.

Best Regards,

Keita

Labels (3)
0 Kudos
Reply
1 Solution
1,755 Views
Yuri
NXP Employee
NXP Employee

Keita, hello !

  Yes, You are right : “SCKT and FST should connect to ESAI_TX_CLK
and ESAI_TX_FS”.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
1,756 Views
Yuri
NXP Employee
NXP Employee

Keita, hello !

  Yes, You are right : “SCKT and FST should connect to ESAI_TX_CLK
and ESAI_TX_FS”.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,755 Views
keitanagashima
Senior Contributor I

Thanks Yuri!

OK. I got it.

Best Regards,

Keita

0 Kudos
Reply