About ESAI slave connection in i.MX6DQ.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About ESAI slave connection in i.MX6DQ.

ソリューションへジャンプ
2,067件の閲覧回数
keitanagashima
Senior Contributor I

Dear All,

Hello.

I have a question about ESAI slave connection in i.MX6DQ.

Refer to attached file and please check the clock connection.

Best Regards,

Keita

ラベル(3)
0 件の賞賛
返信
1 解決策
1,928件の閲覧回数
Yuri
NXP Employee
NXP Employee

Keita, hello !

  Yes, You are right : “SCKT and FST should connect to ESAI_TX_CLK
and ESAI_TX_FS”.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,929件の閲覧回数
Yuri
NXP Employee
NXP Employee

Keita, hello !

  Yes, You are right : “SCKT and FST should connect to ESAI_TX_CLK
and ESAI_TX_FS”.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,928件の閲覧回数
keitanagashima
Senior Contributor I

Thanks Yuri!

OK. I got it.

Best Regards,

Keita

0 件の賞賛
返信