Dear All,
Refer to ERR004365 in IMX6DQCE(Rev.6).
Projected Impact is "EIM does not support exclusive accesses according to AXI specifications."
[Questions]
1. Is there a use case of exclusive accesses in BSP (jb4.2.2_1.0.0)?
2. I think that the user doesn't need to care the AXI bus access.
How implement the workaround to avoid the exclusive accesses?
Best Regards,
Keita
已解决! 转到解答。
Hello,
ARM provides exclusive access functionality via the LDREX/STREX pair of instructions.
NXP Android does not use this mechanism for EIM.
To avoid the issue customers also should not use these exclusive accesses for EIM in their
applications and drivers.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello,
ARM provides exclusive access functionality via the LDREX/STREX pair of instructions.
NXP Android does not use this mechanism for EIM.
To avoid the issue customers also should not use these exclusive accesses for EIM in their
applications and drivers.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------