Dear All,
Hello. I have questions about EDID of HDMI TX, we met some problems.
Background:
i.MX6D (MCIMX6D6AVT10AD) chip is used.
Please refer to below hardware connection. Config of pins is as followed:
- MX6Q_PAD_EIM_EB2__HDMI_TX_DDC_SCL
- MX6Q_PAD_EIM_D16__HDMI_TX_DDC_SDA
When we read EDID of HDMI sink device though HDMI_TX_DDC method, no signal is found on SCL & SDA.
Questions:
1) On MCIMX6D6AVT10AD chip (on which HDCP encryption is disabled), can we use HDMI_TX_DDC method, rather than common I2C method, to read EDID of HDMI sink device?
2) If HDMI_TX_DDC method can be used, could you please help us to check how to solve the problem of no signal on SCL & SDA?
Best Regards,
Keita
Solved! Go to Solution.
Hi,
Which BSP are you using? accoridng to FabioEstevam in this previous link HDMI DDC on linux-fslc/mainline with i.MX6
In Kernle 3.16, DDC works fine on some boards Iike mx6qsabresd, cuboxi, wandboard. I wonder if you have checked it out.
Best Regards,
Alejandro
Hi,
Which BSP are you using? accoridng to FabioEstevam in this previous link HDMI DDC on linux-fslc/mainline with i.MX6
In Kernle 3.16, DDC works fine on some boards Iike mx6qsabresd, cuboxi, wandboard. I wonder if you have checked it out.
Best Regards,
Alejandro