About DVFS register for i.MX7solo

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About DVFS register for i.MX7solo

901 Views
yuuki
Senior Contributor II

Daer all,

I think that i.MX7solo has DVFS function
However, I cannot find a register in conjunction with DVFS in Reference Manual.

(IMX7SRM Rev. 0.1, 08/2016)

Does i.MX7Solo have the HW DVFS function that can be set in registers?

Best Regards,
Yuuki

Labels (1)
0 Kudos
Reply
1 Reply

793 Views
art
NXP Employee
NXP Employee

No, the i.MX7Solo processor doesn't have any dedicated register to implement the DVFS function. The voltage scaling operation is performed using the integrated Power Management Unit (PMU) module together with external Power Management IC (PMIC). The frequency scaling operation is performed using the integrated Clock Controller Module (CCM). Most of the sense and control functions of the DVFS algorithm are implemented in software.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply