About DMA of ECSPI

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,386件の閲覧回数
takashitakahash
Contributor III

Hi community.

Our customer has below question.

About DMA of ECSPI,
ECSPI by Configu to SPI of the Master, so it is to transmit only.
( Receive is not performed).

TXFIFO side, as to send data using DMA,
RXFIFO side, ignoring overflow, sending doesn't matter?

(For example, Disable to RXFIFO Overflow Interrupt , do not affect the TX processing?)

ラベル(1)
0 件の賞賛
返信
1 解決策
1,264件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

you are right, RX side can be ignored, possibly disabling

RXFIFO Overflow Interrupt. This should not affect TX processing.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,265件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

you are right, RX side can be ignored, possibly disabling

RXFIFO Overflow Interrupt. This should not affect TX processing.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信