About DDR3 connection in i.MX6DL.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About DDR3 connection in i.MX6DL.

ソリューションへジャンプ
2,155件の閲覧回数
keitanagashima
Senior Contributor I

Hi, Sir or Madam,

Refer to schematic of  i.MX6DL SABRE-SDP.

i.MX6DL connected to 2Gb_DDR3(16bit width) x4.

Is i.MX6DL possible to connect to 4Gb_DDR3(8bit width) x4?

Best Regards,

Keita

ラベル(3)
0 件の賞賛
返信
1 解決策
2,047件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Keita

yes, with i.MX6DL it is possible to connect to 4Gb_DDR3(8bit width) x4.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,048件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Keita

yes, with i.MX6DL it is possible to connect to 4Gb_DDR3(8bit width) x4.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,047件の閲覧回数
keitanagashima
Senior Contributor I

Dear chipexpert,

Thank you for your prompt reply.

OK. Thank you.

Keita

0 件の賞賛
返信