About DDR3 connection in i.MX6DL.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About DDR3 connection in i.MX6DL.

跳至解决方案
1,902 次查看
keitanagashima
Senior Contributor I

Hi, Sir or Madam,

Refer to schematic of  i.MX6DL SABRE-SDP.

i.MX6DL connected to 2Gb_DDR3(16bit width) x4.

Is i.MX6DL possible to connect to 4Gb_DDR3(8bit width) x4?

Best Regards,

Keita

标签 (3)
0 项奖励
回复
1 解答
1,794 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Keita

yes, with i.MX6DL it is possible to connect to 4Gb_DDR3(8bit width) x4.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,795 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Keita

yes, with i.MX6DL it is possible to connect to 4Gb_DDR3(8bit width) x4.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,794 次查看
keitanagashima
Senior Contributor I

Dear chipexpert,

Thank you for your prompt reply.

OK. Thank you.

Keita

0 项奖励
回复