About DDR3 connection in i.MX6DL.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About DDR3 connection in i.MX6DL.

Jump to solution
716 Views
keitanagashima
Senior Contributor I

Hi, Sir or Madam,

Refer to schematic of  i.MX6DL SABRE-SDP.

i.MX6DL connected to 2Gb_DDR3(16bit width) x4.

Is i.MX6DL possible to connect to 4Gb_DDR3(8bit width) x4?

Best Regards,

Keita

Labels (3)
0 Kudos
1 Solution
608 Views
igorpadykov
NXP Employee
NXP Employee

Hi Keita

yes, with i.MX6DL it is possible to connect to 4Gb_DDR3(8bit width) x4.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
2 Replies
609 Views
igorpadykov
NXP Employee
NXP Employee

Hi Keita

yes, with i.MX6DL it is possible to connect to 4Gb_DDR3(8bit width) x4.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
608 Views
keitanagashima
Senior Contributor I

Dear chipexpert,

Thank you for your prompt reply.

OK. Thank you.

Keita

0 Kudos