About DDR_SEL setting of IOMUXC_SW_PAD_CTL_GRP_DDR_TYPE on i.MX6Solo

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About DDR_SEL setting of IOMUXC_SW_PAD_CTL_GRP_DDR_TYPE on i.MX6Solo

Jump to solution
1,173 Views
yuuki
Senior Contributor II

Dear all,

We want to know the DDR_SEL setting of the IOMUXC_SW_PAD_CTL_GRP_DDR_TYPE register.

For the DDR_SEL of the IOMUXC_SW_PAD_CTL_PAD_DRAM_RESET register, we found the following URL.
https://community.freescale.com/message/360650#360650

According to this, DDR_SEL should be set in "00"


For the DDR_SEL of the IOMUXC_SW_PAD_CTL_GRP_DDR_TYPE register, we want to know  whether the same setting is necessary.

Must this DDR_SEL be set in "00", too?

Best Regards,

Yuuki

Labels (2)
0 Kudos
1 Solution
743 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

DDR_SEL of the IOMUXC_SW_PAD_CTL_GRP_DDR_TYPE register

should be set according to description in RM:

10 LPDDR2

11 DDR3

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
2 Replies
743 Views
andrewdyer
Contributor III

see also  imx6 DDR_SEL

744 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

DDR_SEL of the IOMUXC_SW_PAD_CTL_GRP_DDR_TYPE register

should be set according to description in RM:

10 LPDDR2

11 DDR3

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos