Dear all,
We want to confirm some pins of i.MX7Solo.
In "Table 96. i.MX 7Solo 19 × 19 mm, 0.75 mm pitch ball map" in Datasheet (IMX7SCEC Rev. 4, 04/2017),
"D3 : SD2_CD_B" and "AD5 : Vss" are explained.
However, these pins are not explained in "Table 94. i.MX 7Solo 19 x 19 mm supplies contact assignments" and "Table 95. i.MX 7Solo 19 x 19 mm functional contact assignments".
We understand that a description of Table 96 is right.
Is our understanding right?
Please tell me the right contents when it is wrong.
Best Regards,
Yuuki
Solved! Go to Solution.
Thank you for this information.
As Yuri has indicated, Table 96 is correct. This information has been added to the shared review. and will be published in revision 6.
mark
Thank you for this information.
As Yuri has indicated, Table 96 is correct. This information has been added to the shared review. and will be published in revision 6.
mark
Hello,
Yes, description of Table 96 is right. I informed the team about lack information about pins
D3 and AD5 (AD05). It should be corrected in next documentation rev.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------