About D3 pin and AD5 pin for i.MX7Solo

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About D3 pin and AD5 pin for i.MX7Solo

Jump to solution
609 Views
yuuki
Senior Contributor II

Dear all,

We want to confirm some pins of i.MX7Solo.

In "Table 96. i.MX 7Solo 19 × 19 mm, 0.75 mm pitch ball map" in Datasheet (IMX7SCEC Rev. 4, 04/2017),
"D3 : SD2_CD_B" and "AD5 : Vss" are explained.

However, these pins are not explained in "Table 94. i.MX 7Solo 19 x 19 mm supplies contact assignments" and "Table 95. i.MX 7Solo 19 x 19 mm functional contact assignments".

We understand that a description of Table 96 is right.

Is our understanding right?
Please tell me the right contents when it is wrong.

Best Regards,
Yuuki

Labels (1)
Tags (4)
0 Kudos
1 Solution
541 Views
markruthenbeck
NXP Employee
NXP Employee

Thank you for this information.

As Yuri has indicated, Table 96 is correct. This information has been added to the shared review. and will be published in revision 6.

mark

View solution in original post

0 Kudos
2 Replies
542 Views
markruthenbeck
NXP Employee
NXP Employee

Thank you for this information.

As Yuri has indicated, Table 96 is correct. This information has been added to the shared review. and will be published in revision 6.

mark

0 Kudos
541 Views
Yuri
NXP Employee
NXP Employee

Hello,

   Yes, description of Table 96 is right. I informed the team about lack information about pins

D3 and AD5 (AD05). It should be corrected in next documentation rev.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos