About Cortex-A9 ARM Errata 845369 for i.MX 6Solo and 6SoloX.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About Cortex-A9 ARM Errata 845369 for i.MX 6Solo and 6SoloX.

Jump to solution
1,175 Views
keitanagashima
Senior Contributor I

Dear All,

Hello. The errata had already discussed below community.

Cortex-A9 ARM Errata 845369

Refer to Cortex-A9 errata (ARM Cortex-A9 processors r4 releases Software Developers Errata Notice).

-----

This erratum affects configurations with either:

• One processor if the ACP is present

• Two or more processors

-----

[Question]

Does this errata affect i.MX 6Solo and 6SoloX?

Best Regards,

Keita

Labels (2)
0 Kudos
Reply
1 Solution
789 Views
igorpadykov
NXP Employee
NXP Employee

Hi Keita

no, this erratum does not affect i.MX 6Solo and 6SoloX.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
790 Views
igorpadykov
NXP Employee
NXP Employee

Hi Keita

no, this erratum does not affect i.MX 6Solo and 6SoloX.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply