About CodeAurora

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About CodeAurora

跳至解决方案
3,454 次查看
funatsu
Contributor I

Hi all,

I have a question about CodeAurora.

According to the following two threads,

https://community.nxp.com/thread/323782

https://community.nxp.com/thread/499539

CodeAurora is the Freescale Official Release BSP and it is static, does not include bug fixes, apparently.

However, it seems https://source.codeaurora.org/external/imx is updated frequently.

I am going to use i.mx8 mini but I cannot see which BSPs I should use,

I mean I don't know which of the following repositories I should use,

https://github.com/Freescale/fsl-community-bsp-platform

https://source.codeaurora.org/external/imx

Can anyone tell me the difference between them?

0 项奖励
回复
1 解答
3,164 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Takao

>However, it seems https://source.codeaurora.org/external/imx is updated frequently.

right, for example one can look at "commits" :

pastedImage_2.jpg

 

>I am going to use i.mx8 mini but I cannot see which BSPs I should use,

supported processors are listed in Release Notes document p.1 available on

documentation link i.MX Software and Development Tools | NXP 

>I mean I don't know which of the following repositories I should use,

it is necessary to use source.codeaurora.org/external/imx/linux-imx  repository

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
3,164 次查看
funatsu
Contributor I

Hi igor

Thank you for your answer.

0 项奖励
回复
3,165 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Takao

>However, it seems https://source.codeaurora.org/external/imx is updated frequently.

right, for example one can look at "commits" :

pastedImage_2.jpg

 

>I am going to use i.mx8 mini but I cannot see which BSPs I should use,

supported processors are listed in Release Notes document p.1 available on

documentation link i.MX Software and Development Tools | NXP 

>I mean I don't know which of the following repositories I should use,

it is necessary to use source.codeaurora.org/external/imx/linux-imx  repository

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复