About CS1 on Port A of QuadSPI configuration parameters

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About CS1 on Port A of QuadSPI configuration parameters

ソリューションへジャンプ
3,400件の閲覧回数
goto11
Contributor III

Hello,

 

I am using QSPI_A to access memory.
Since the QSPI_A_SS0_B and QSPI_A_SS1_B signals are Chip select1 port0/1 deviceA, shouldn't CS1 on Port A be set to enable?
The designer says that CS1 on Port A can be accessed with the disable setting.
Is there any problem with this setting?

 

Regards,

Goto

ラベル(1)
0 件の賞賛
返信
1 解決策
3,366件の閲覧回数
Yuri
NXP Employee
NXP Employee
0 件の賞賛
返信
7 返答(返信)
3,391件の閲覧回数
Yuri
NXP Employee
NXP Employee

@goto11 
Hello,


   QSPI_A_SS0_B may be used without QSPI_A_SS1_B.
Section 10.2.8.2 (Dual Die Flashes) of i.MX 7Dual Reference
Manual (Rev. 1, 01/2018) describes configuration, where
both signals are applied.

 

Regards,
Yuri.

0 件の賞賛
返信
3,387件の閲覧回数
goto11
Contributor III

Hello,

 

It's not the answer to what I asked.
Is the QSPI_A_SS0_B(QSPI_A_SS1_B) signal valid when the CS1 on Port A setting in Table 6-50 (QuadSPI configuration parameters) is disabled?

Regards,

Goto

0 件の賞賛
返信
3,385件の閲覧回数
Yuri
NXP Employee
NXP Employee

@goto11 

  The QSPI_A_SS0_B signal is valid when the CS1 on Port A setting in QuadSPI configuration parameters is disabled. QSPI_A_SS1_B is not configured for QSPI in such case.

~Yuri.

0 件の賞賛
返信
3,380件の閲覧回数
goto11
Contributor III

Hello,

When the setting value of "CS1 on Port A" in Table 6-50 (QuadSPI configuration parameters) is disabled, is it not possible to use Flash A2 with the following configuration?

無題.png

Regards,

Goto

0 件の賞賛
返信
3,376件の閲覧回数
Yuri
NXP Employee
NXP Employee

@goto11 

 if "CS1 on Port A" in  QuadSPI configuration parameters is disabled, 
it is not possible to use the Flash A2.

0 件の賞賛
返信
3,374件の閲覧回数
goto11
Contributor III

If the setting value of "CS1 on Port A" in Table 6-50 (QuadSPI configuration parameters) is enable, can Flash A2 with the following configuration be used?

0 件の賞賛
返信
3,367件の閲覧回数
Yuri
NXP Employee
NXP Employee

@goto11 

 

  yes.

0 件の賞賛
返信