Dear all,
I am referring to the following.
MCIMX28RM.pdf (Rev2):
- 27.5.4 I2C Timing Register 2 (HW_I2C_TIMING2)(P.1895)
I cannot understand BUS_FREE and the LEADIN_COUNT field of HW_I2C_TIMING2 well.
What kind of influence do these fields have on I2C waveform?
May I have advice?
Best Regards,
Solved! Go to Solution.
As for the BUS_FREE bit field, please refer to IC9 (bus free time between a STOP
and START condition) timing parameter in i.MX28 Datasheet (Hardware Specs).
LEADIN_COUNT relates to IC2 parameter.
Also, please take a look at Table 2-18 (I2C Timing Parameters) of the i.MX23
Reference Manual.
http://cache.freescale.com/files/dsp/doc/ref_manual/IMX23RM.pdf
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
As for the BUS_FREE bit field, please refer to IC9 (bus free time between a STOP
and START condition) timing parameter in i.MX28 Datasheet (Hardware Specs).
LEADIN_COUNT relates to IC2 parameter.
Also, please take a look at Table 2-18 (I2C Timing Parameters) of the i.MX23
Reference Manual.
http://cache.freescale.com/files/dsp/doc/ref_manual/IMX23RM.pdf
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------