About BCLK toggle with synchronous access in i.MX6DQ.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About BCLK toggle with synchronous access in i.MX6DQ.

Jump to solution
1,024 Views
keitanagashima
Senior Contributor I

Dear All,

I have a question about BCLK toggles with synchronous access in i.MX6DQ.

Refer to Page.1019 in IMX6DQRM(Rev.2).

====

The BCLK signal toggles only when burst access is executed toward the external device (BCM=1'b0 for normal mode use).

====

We assume the single read / write and burst transfer with sync access (BCM=0).

In case of single read / write, does BCLK signal toggle (output)?

Best Regards,

Keita

Labels (5)
0 Kudos
Reply
1 Solution
930 Views
igorpadykov
NXP Employee
NXP Employee

Hi Keita

BCM.jpg

>We assume the single read / write and burst transfer with sync access (BCM=0).

>In case of single read / write, does BCLK signal toggle (output)?

yes, at synchronous access BCLK signal toggles even in case of single

beat burst.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
931 Views
igorpadykov
NXP Employee
NXP Employee

Hi Keita

BCM.jpg

>We assume the single read / write and burst transfer with sync access (BCM=0).

>In case of single read / write, does BCLK signal toggle (output)?

yes, at synchronous access BCLK signal toggles even in case of single

beat burst.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply