Dear All,
Hello.
Which grade is AEC-Q100 supporting for i.MX 6SoloX (auto qual)?
Grade 1, 2, or 3?
Best Regards,
Keita
Solved! Go to Solution.
Dear gusarambula ,
Hello.
I got the below answer from local marketing team.
i.MX6SoloX supports the AEC-Q100 grade 3.
Best Regards,
Keita
Hello Keita,
I am making some research with our marketing team to validate the information. I get back to you as soon as I get a response.
Dear James,
Hello.Thank you for your support.
My customer is very hurry for this question.
Please answer it asap.
Best Regards,
Keita
Hello Keita Nagashima,
We're sorry for the delay. We're yet to receive confirmation on the grade AEC-Q100 qualification for the i.MX6SX. However, the i.MX6S/DL/D/Q Automotive parts have a AEC-Q100 Grade 3 qualification so I would expect the same grade for the i.MX6SoloX Auto.
As soon as we have the information double checked we'll let you know.
Dear gusarambula,
Thank you for your reply.
> the i.MX6S/DL/D/Q Automotive parts have a AEC-Q100 Grade 3 qualification
OK. I got it.
> so I would expect the same grade for the i.MX6SoloX Auto.
I think so, too.
OK. I'll wait your answer.
Best Regards,
Keita
Hello Keita Nagashima,
Thanks for your patience.
Finally, just for reference the temperature grades for AEC-Q100 qualification are as follow:
Grade 0: -40°C to +150°C ambient operating temperature range
Grade 1: -40°C to +125°C ambient operating temperature range
Grade 2: -40°C to +105°C ambient operating temperature range
Grade 3: -40°C to +85°C ambient operating temperature range
Grade 4: 0°C to +70°C ambient operating temperature range
Dear gusarambula ,
Hello.
I got the below answer from local marketing team.
i.MX6SoloX supports the AEC-Q100 grade 3.
Best Regards,
Keita
Hi gusarambula,
> I confirmed and the i.MX6SX Automotive parts can reach -40C to +125C, which is AEC-Q100 Grade 1.
> The same for our i.MX6S/DL/D/Q Automotive parts (I'm sorry for the incorrect information earlier).
Really?
i.MX6SX is defined at the junction temperature (-40C to +125C).
But, AEC-Q100 grade is defined at the ambient temperature!
I think that Junction temperature and Ambient one should have temperature difference.
Please check again.
Best Regards,
Keita