About AEC-Q100 supporting for i.MX 6SoloX (auto qual)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About AEC-Q100 supporting for i.MX 6SoloX (auto qual)

跳至解决方案
1,092 次查看
keitanagashima
Senior Contributor I

Dear All,

Hello.

Which grade is AEC-Q100 supporting for i.MX 6SoloX (auto qual)?

Grade 1, 2, or 3?

Best Regards,

Keita

标签 (1)
1 解答
796 次查看
keitanagashima
Senior Contributor I

Dear gusarambula ,

Hello.

I got the below answer from local marketing team.

i.MX6SoloX supports the AEC-Q100 grade 3.

Best Regards,

Keita

在原帖中查看解决方案

7 回复数
796 次查看
jamesbone
NXP TechSupport
NXP TechSupport

Hello Keita,

I am making some research with our marketing team to validate the information.  I get back to you as soon as I get a response.

0 项奖励
796 次查看
keitanagashima
Senior Contributor I

Dear James,

Hello.Thank you for your support.

My customer is very hurry for this question.

Please answer it asap.

Best Regards,

Keita

0 项奖励
796 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Keita Nagashima,

We're sorry for the delay. We're yet to receive confirmation on the grade AEC-Q100 qualification for the i.MX6SX. However, the i.MX6S/DL/D/Q Automotive parts have a AEC-Q100 Grade 3 qualification so I would expect the same grade for the i.MX6SoloX Auto.

As soon as we have the information double checked we'll let you know.

0 项奖励
796 次查看
keitanagashima
Senior Contributor I

Dear gusarambula,

Thank you for your reply.

> the i.MX6S/DL/D/Q Automotive parts have a AEC-Q100 Grade 3 qualification

OK. I got it.

> so I would expect the same grade for the i.MX6SoloX Auto.

I think so, too.

OK. I'll wait your answer.

Best Regards,

Keita

0 项奖励
796 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Keita Nagashima,

Thanks for your patience.

Finally, just for reference the temperature grades for AEC-Q100 qualification are as follow:

Grade 0: -40°C to +150°C ambient operating temperature range

Grade 1: -40°C to +125°C ambient operating temperature range

Grade 2: -40°C to +105°C ambient operating temperature range

Grade 3: -40°C to +85°C ambient operating temperature range

Grade 4: 0°C to +70°C ambient operating temperature range

0 项奖励
797 次查看
keitanagashima
Senior Contributor I

Dear gusarambula ,

Hello.

I got the below answer from local marketing team.

i.MX6SoloX supports the AEC-Q100 grade 3.

Best Regards,

Keita

796 次查看
keitanagashima
Senior Contributor I

Hi gusarambula,

> I confirmed and the i.MX6SX Automotive parts can reach -40C to +125C, which is AEC-Q100 Grade 1.

> The same for our i.MX6S/DL/D/Q Automotive parts (I'm sorry for the incorrect information earlier).

Really?

i.MX6SX  is defined at the junction temperature (-40C to +125C).

But, AEC-Q100 grade is defined at the ambient temperature!

AEC-Q100 grade.PNG

I think that Junction temperature and Ambient one should have temperature difference.

Please check again.

Best Regards,

Keita

0 项奖励