AVB demo board selection and purchase

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

AVB demo board selection and purchase

Jump to solution
722 Views
LiaoPanther
Contributor I

Hi NXP,
I want to setup an AVB demo project to evaluate the AVB and automotive Ethernet technology, my requirements are as follows:

1.Demonstrate the AVB synchronization mechanism. That is, there are two ECUs to display from the same video/audio source(Such as computer or a camera), and they are perfectly synchronized in the sreen.

2.Evaluate other automotive Ethernet technology such as SOA(Service Oriented Architecture), so traditional TCP/IP stack is still required.

3.RTOS development environment is preferred.(Maybe we don't want to learn Linux)
I have researced the hardware source from NXP and I think maybe SABRE platform will fulfil my requirements, so I made the following selection:

1. CPU base board: MCIMXABASEV1 

2. CPU card: MCIMX6DLAICPU2 ( i.MX 6DualLite/6Solo)

3. Ethernet card: IMXAI2ETH-BRC (Broadcom Ethernet)

(Because I need to simulate two ECUs, I will purchase two pieces for item 1,2,3)

4.Ethernet switch:SJA1105Q-EVB (Used for AVB stream data switch)

5.Ethernet port convertor:RDDRONE-T1ADAPT (If the data source comes from my laptop, I need a convertor to convert RJ45 to 100 Base-T1 connector)

My question are as follows:

1.Is my hardware selection correct to fulfil my requirements?

2.After I purchased these EVBs listed above, where can I get the AVB stack software?

3.Is any technical support can be provided after I make the purchase?

Thanks.

0 Kudos
1 Solution
696 Views
jamesbone
NXP TechSupport
NXP TechSupport

Hello,

 

Regarding your questions

 

1.Is my hardware selection correct to fulfil my requirements?

ANSWER.  Yes, you have the correct hardware selection.

2.After I purchased these EVBs listed above, where can I get the AVB stack software?

ANSWER.  The AVB Stack, it is license separately, please contact your local sales, to get a quote depending on your requirement of licenses.

3.Is any technical support can be provided after I make the purchase?

ANSWER.  Yes, we have offer Pro Support for this License Software pack.

 

View solution in original post

0 Kudos
1 Reply
697 Views
jamesbone
NXP TechSupport
NXP TechSupport

Hello,

 

Regarding your questions

 

1.Is my hardware selection correct to fulfil my requirements?

ANSWER.  Yes, you have the correct hardware selection.

2.After I purchased these EVBs listed above, where can I get the AVB stack software?

ANSWER.  The AVB Stack, it is license separately, please contact your local sales, to get a quote depending on your requirement of licenses.

3.Is any technical support can be provided after I make the purchase?

ANSWER.  Yes, we have offer Pro Support for this License Software pack.

 

0 Kudos