AVB , The sounds played on the AVB host are not synchronize with those played in other AVB endpoint

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

AVB , The sounds played on the AVB host are not synchronize with those played in other AVB endpoint

1,103 Views
ZenJeams
Contributor I

hi NXP teams,

I try to use IMX8MP master board(Real-time_Edge_v2.5 system) capture audio data from UAC, the audio data is just simply playback locally, as well as transmitted over AVB network and then received/playback by other AVB endpoints.

Actually, the sounds played on the AVB host are not synchronize with those played in other AVB endpoints

How to synchronize the “playback” action between AVB & non-AVB traffics?

0 Kudos
Reply
2 Replies

1,058 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @ZenJeams 

Which ethernet port you are using?

You can refer this knowledge base:

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/AVB-TSN-demo-on-i-MX8MP/ta-p/1123791#toc...

0 Kudos
Reply

1,017 Views
ZenJeams
Contributor I

I using  genavb-media-app in NXP/GenAVB-TSN (git-5.4 branch) project, and using  IMX8MP  board ethernet  1 port as AVB endpoint.

0 Kudos
Reply