Hi,
I am using iMX25 PDK with MT29F2G08ABAEAWP Nand flash. I would like to know whether anyone has the modified / configured ATK tool that supports the above mentioned device for downloading. I am trying to modify on my own with the source code of ATK tool available, but without any success till now. Kindly help me to download uboot, image and file system in to the above flash using ATK tool.
Thanks,
Arumugam R
I had to make sure the details were in both nand_device_info_table_type_2 and nand_device_info_table_type_7 to get it to work.
Generally recent ATK releases should define NAND type automatically via NAND ID.
And there is corresponding information for the NAND flash "MT29F2G08ABAEAWP:E" in
"nand_device_info.c" (from ATK sources).
Please double check parameters "BI Swap" and "BBT", what were used to erase the NAND (via ATK). Also please pay attention if NAND signal RDY is pulled up via a resistor of ~10 KOhm.