ARM DS-5 support for Sabre board (not Sabre lite which is supported)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ARM DS-5 support for Sabre board (not Sabre lite which is supported)

622 Views
EricCowden
Contributor IV

It looks like ARMs DS-5 tools only offer SOC level support for the Sabre platform and not board level support.   They only support board level features on the Sabre Lite from Boundary Devices.    Does anyone have a profile or database to enable the Freescale Sabre board level support with ARMs DS-5 tools?

Labels (1)
0 Kudos
1 Reply

376 Views
SergioSolis
NXP Employee
NXP Employee

We did tried connecting the DS-5 to a SABRE-SD board in the past and we were able to do so at least for u-boot debugging.

We realized that the latest DS-5 release already has i.MX6 support, but when we actually achieved connecting we were using version 5.14 and added support using the cdbimporter application (original rvc file attached).

0 Kudos