Hi,
Can anyone provide me the ARM compiler startup(Cortex-M4 or Cortex-A9)files for IMX6SX SBD board.
or
Send me serial driver for IMX6SX SBD board which should compile using ARM C compiler 5/6 (DS-5 ARM compilers).
Regards,
Raghavendra
Hi,
For i.MX6SX, you could take a look to Linux and Android BSPs for A9 core, and to the FreeRTOS and bare-metal examples for M4 core at the following link:
The FreeRTOS BSP installation also includes the bare-metal examples (UART included), supporting IAR, DS5 and ARMGCC IDEs; please refer to the following route considering the instlation folder of FreeRTOS for i.MX6SX BSP:
…\FreeRTOS_BSP_1.0.0_iMX6SX\examples\imx6sx_sdb_m4\driver_examples\uart_imx
Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------