APBH DMA and GPMI Interrupts

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

APBH DMA and GPMI Interrupts

999 Views
jaysherritt
Contributor I

Hi,

I'm writing a device driver for NAND Flash for the i.MX 6 (DQ), and would like to have it be fully interrupt driven.  The documentation for the APBH_DMA in the reference manual (14.5.2) states "Each channel has a dedicated interrupt vector in the vectored interrupt controller.", however, I'm unable to find these in the interrupt map, and my read of the Linux driver is that it only uses interrupts to indicate the end of transfers where the BCH encoding is enabled.

The CHxCMDCMPLT_IRQ bit(s) in the APBH_CTRL1n register are being set appropriately in accordance with my channel commands (and enabled by the CHxCMDCMPLT_IRQ_EN bits), but I haven't found any way to promulgate these back to the GIC.

How do I get an interrupt at the end of a descriptor phase when BCH encoding or decoding is not enabled?

Thanks.

Jay

Labels (2)
0 Kudos
Reply
1 Reply

729 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Please refer to Table 3-1 (ARM domain interrupt summary),

where IRQ 45 as “APBH-Bridge-DMA Logical OR of APBH-Bridge-DMA

channels 0-3 completion and error interrupts” is shown.

  It is needed to check interrupt request status bits in APBH_CTRL1n to define

source of the event in ISR. 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply