AOSP Build failed after clean the source

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

AOSP Build failed after clean the source

5,330 次查看
vinothkumars
Senior Contributor IV

Hi,

I got build error once done the clean the source,

Platform : Android 9 Automotive with iMX8QM-MEK

[ 0% 385/94752] Building arm64 4.14 kernel ...
FAILED: out/target/product/mek_8q/obj/KERNEL_OBJ/arch/arm64/boot/Image.lz4
/bin/bash -c "(PATH=\$PATH make -j2 SHELL=/bin/bash -C vendor/nxp-opensource/kernel_imx mrproper ) && (PATH=\$(cd prebuilts/misc/linux-x86/lz4; pwd):\$PATH CCACHE_NODIRECT=\"true\" make -j2 SHELL=/bin/bash -C vendor/nxp-opensource/kernel_imx O=\$(/home/emb-vinosek/Documents/VINOTH/IndiEV-IMX8-A9/source/prebuilts/build-tools/linux-x86/bin/ckati --realpath out/target/product/mek_8q/obj/KERNEL_OBJ 2> /dev/null) ARCH=arm64 CROSS_COMPILE=\" /home/emb-vinosek/Documents/VINOTH/IndiEV-IMX8-A9/source/prebuilts/gcc/linux-x86/aarch64/aarch64-linux-android-4.9/bin/aarch64-linux-androidkernel-\" KCFLAGS=\"\" KAFLAGS=\"\" Image.lz4 ) && (PATH=\$(cd prebuilts/misc/linux-x86/lz4; pwd):\$PATH CCACHE_NODIRECT=\"true\" make -j2 SHELL=/bin/bash -C vendor/nxp-opensource/kernel_imx O=\$(/home/emb-vinosek/Documents/VINOTH/IndiEV-IMX8-A9/source/prebuilts/build-tools/linux-x86/bin/ckati --realpath out/target/product/mek_8q/obj/KERNEL_OBJ 2> /dev/null) ARCH=arm64 CROSS_COMPILE=\" /home/emb-vinosek/Documents/VINOTH/IndiEV-IMX8-A9/source/prebuilts/gcc/linux-x86/aarch64/aarch64-linux-android-4.9/bin/aarch64-linux-androidkernel-\" KCFLAGS=\"\" KAFLAGS=\"\" modules )"
make: Entering directory '/home/emb-vinosek/Documents/VINOTH/IndiEV-IMX8-A9/source/vendor/nxp-opensource/kernel_imx'
make: Leaving directory '/home/emb-vinosek/Documents/VINOTH/IndiEV-IMX8-A9/source/vendor/nxp-opensource/kernel_imx'
make: Entering directory '/home/emb-vinosek/Documents/VINOTH/IndiEV-IMX8-A9/source/vendor/nxp-opensource/kernel_imx'
make[1]: Entering directory '/home/emb-vinosek/Documents/VINOTH/IndiEV-IMX8-A9/source/out/target/product/mek_8q/obj/KERNEL_OBJ'
GEN ./Makefile
HOSTCC scripts/kconfig/zconf.tab.o
scripts/kconfig/zconf.tab.c:2466:23: fatal error: zconf.lex.c: No such file or directory
compilation terminated.
scripts/Makefile.host:119: recipe for target 'scripts/kconfig/zconf.tab.o' failed
make[3]: *** [scripts/kconfig/zconf.tab.o] Error 1
/home/emb-vinosek/Documents/VINOTH/IndiEV-IMX8-A9/source/vendor/nxp-opensource/kernel_imx/Makefile:522: recipe for target 'silentoldconfig' failed
make[2]: *** [silentoldconfig] Error 2
make[1]: *** No rule to make target 'include/config/auto.conf', needed by 'include/config/kernel.release'. Stop.
make[1]: Leaving directory '/home/emb-vinosek/Documents/VINOTH/IndiEV-IMX8-A9/source/out/target/product/mek_8q/obj/KERNEL_OBJ'
Makefile:146: recipe for target 'sub-make' failed
make: *** [sub-make] Error 2
make: Leaving directory '/home/emb-vinosek/Documents/VINOTH/IndiEV-IMX8-A9/source/vendor/nxp-opensource/kernel_imx'
[ 0% 386/94752] target thumb C++: libv8src_32 <= external/v8/src/api.cc
[ 0% 387/94752] target thumb C++: libv8src_32 <= external/v8/src/ast/ast-function-literal-id-reindexer.cc
[ 0% 388/94752] target thumb C++: libv8src_32 <= external/v8/src/ast/ast-expression-rewriter.cc
[ 0% 389/94752] target thumb C++: libv8src_32 <= external/v8/src/ast/ast-value-factory.cc
[ 0% 390/94752] target thumb C++: libv8src_32 <= external/v8/src/ast/ast.cc
ninja: build stopped: subcommand failed.
11:04:52 ninja failed with: exit status 1

#### failed to build some targets (04:12 (mm:ss)) ####

Steps,

source build/envsetup.sh

lunch 36

make clean

source build/envsetup.sh

lunch 36

make -j6

Thanks & Regards,

VinothS,

Regards,
Vinothkumar Sekar
0 项奖励
回复
3 回复数

4,929 次查看
vinothkumars
Senior Contributor IV

Fixed.

Regards,
Vinothkumar Sekar
0 项奖励
回复

4,833 次查看
Ketki
Contributor I

How did you solve this issue ? I have similar problem . zconf.lex.c not found . Though there is a zconf.lex.c_shipped file

0 项奖励
回复

4,929 次查看
diegoadrian
NXP Employee
NXP Employee

Hello,

Unfortunately, we cannot support Android automotive until the i.MX8QM is completely released. Most of our software may be subject to change and we cannot guarantee if it will work. I apologize for the inconvenience this may give you.

Best regards,

Diego.

0 项奖励
回复