Hi,
I have to disable the BatteryService Java class among several references to battery related objects in order to boot Android. It hangs in an boot-loop otherwise.
How can I make AOSP 7 work on my batteryless device? Do I have to write software or should I disable something?
What I've done so far:
I've written a power stub driver that has the options and return static values.
static enum power_supply_property stub_power_charger_props[] = {
POWER_SUPPLY_PROP_ONLINE,
};
static enum power_supply_property stub_power_battery_props[] = {
POWER_SUPPLY_PROP_STATUS,
POWER_SUPPLY_PROP_PRESENT,
POWER_SUPPLY_PROP_CAPACITY,
POWER_SUPPLY_PROP_VOLTAGE_MAX_DESIGN,
POWER_SUPPLY_PROP_VOLTAGE_MIN_DESIGN,
POWER_SUPPLY_PROP_HEALTH,
POWER_SUPPLY_PROP_CAPACITY_LEVEL,
};I've tried to add missing battery stuff in the board config:
device/brand/imx6/imx6.mk: libhealthd.default \
device/brand/imx6/imx6.mk: libbatterymonitor \
device/brand/imx6/imx6.mk: libhealthd_internal \
device/brand/imx6/imx6.mk: healthd \
device/brand/imx6/imx6.mk: batterystats \
device/brand/imx6/imx6.mk: batteryproperties \
device/brand/imx6/imx6.mk: batteryservice \
device/brand/imx6/imx6.mk: libbatteryserviceI even changed system/core/healthd/healthd.cpp so it takes special operations:
diff --git a/system/core/healthd/healthd.cpp b/system/core/healthd/healthd.cpp
index 1c144b34d7..fc431860f3 100644
--- a/system/core/healthd/healthd.cpp
+++ b/system/core/healthd/healthd.cpp
@@ -132,6 +132,13 @@ static struct healthd_mode_ops recovery_ops = {
.battery_update = healthd_mode_nop_battery_update,
};
+static struct healthd_mode_ops touchpoint_ops = {
+ .init = healthd_mode_android_init,
+ .preparetowait = healthd_mode_android_preparetowait,
+ .heartbeat = healthd_mode_nop_heartbeat,
+ .battery_update = healthd_mode_nop_battery_update,
+};
+
static void healthd_mode_nop_init(struct healthd_config* /*config*/) {
}
@@ -366,6 +373,7 @@ int main(int argc, char **argv) {
}
}
}
+ healthd_mode_ops = &touchpoint_ops;
ret = healthd_init();
if (ret) {
I know for sure that an object exists in system/core/healthd/BatteryMonitor.cpp because I've logged the address, thus a BatteryProperties object must exist. However, AOSP complains that "batteryLevel" is called on a null object.
01-01 00:00:28.948 511 546 D VoldConnector: RCV <- {200 27 Command succeeded}
01-01 00:00:28.952 511 511 V UserManagerService: Found /data/user_de/0 with serial number 0
01-01 00:00:28.952 511 511 V UserManagerService: Found /data/user/0 with serial number 0
01-01 00:00:28.953 511 511 V UserManagerService: Found /data/system_de/0 with serial number 0
01-01 00:00:28.958 511 511 I ActivityManager: System now ready
01-01 00:00:28.970 511 511 I SystemServer: Making services ready
01-01 00:00:28.970 511 511 I SystemServiceManager: Starting phase 550
01-01 00:00:28.972 511 511 E System : ******************************************
01-01 00:00:28.973 511 511 E System : ************ Failure starting system services
01-01 00:00:28.973 511 511 E System : java.lang.RuntimeException: Failed to boot service com.android.server.BatteryService: onBootPhase threw an exception during phase 550
01-01 00:00:28.973 511 511 E System : at com.android.server.SystemServiceManager.startBootPhase(SystemServiceManager.java:145)
01-01 00:00:28.973 511 511 E System : at com.android.server.SystemServer$2.run(SystemServer.java:1327)
01-01 00:00:28.973 511 511 E System : at com.android.server.am.ActivityManagerService.systemReady(ActivityManagerService.java:13392)
01-01 00:00:28.973 511 511 E System : at com.android.server.SystemServer.startOtherServices(SystemServer.java:1323)
01-01 00:00:28.973 511 511 E System : at com.android.server.SystemServer.run(SystemServer.java:340)
01-01 00:00:28.973 511 511 E System : at com.android.server.SystemServer.main(SystemServer.java:222)
01-01 00:00:28.973 511 511 E System : at java.lang.reflect.Method.invoke(Native Method)
01-01 00:00:28.973 511 511 E System : at com.android.internal.os.ZygoteInit$MethodAndArgsCaller.run(ZygoteInit.java:890)
01-01 00:00:28.973 511 511 E System : at com.android.internal.os.ZygoteInit.main(ZygoteInit.java:780)
01-01 00:00:28.973 511 511 E System : Caused by: java.lang.NullPointerException: Attempt to read from field 'int android.os.BatteryProperties.batteryLevel' on a null object reference
01-01 00:00:28.973 511 511 E System : at com.android.server.BatteryService.processValuesLocked(BatteryService.java:331)
01-01 00:00:28.973 511 511 E System : at com.android.server.BatteryService.updateBatteryWarningLevelLocked(BatteryService.java:237)
01-01 00:00:28.973 511 511 E System : at com.android.server.BatteryService.onBootPhase(BatteryService.java:218)
01-01 00:00:28.973 511 511 E System : at com.android.server.SystemServiceManager.startBootPhase(SystemServiceManager.java:143)
01-01 00:00:28.973 511 511 E System : ... 8 more
01-01 00:00:28.974 511 511 D AndroidRuntime: Shutting down VM
--------- beginning of crash
01-01 00:00:28.974 511 511 E AndroidRuntime: *** FATAL EXCEPTION IN SYSTEM PROCESS: main
01-01 00:00:28.974 511 511 E AndroidRuntime: java.lang.RuntimeException: Failed to boot service com.android.server.BatteryService: onBootPhase threw an exception during phase 550
01-01 00:00:28.974 511 511 E AndroidRuntime: at com.android.server.SystemServiceManager.startBootPhase(SystemServiceManager.java:145)
01-01 00:00:28.974 511 511 E AndroidRuntime: at com.android.server.SystemServer$2.run(SystemServer.java:1327)
01-01 00:00:28.974 511 511 E AndroidRuntime: at com.android.server.am.ActivityManagerService.systemReady(ActivityManagerService.java:13392)
01-01 00:00:28.974 511 511 E AndroidRuntime: at com.android.server.SystemServer.startOtherServices(SystemServer.java:1323)
01-01 00:00:28.974 511 511 E AndroidRuntime: at com.android.server.SystemServer.run(SystemServer.java:340)
01-01 00:00:28.974 511 511 E AndroidRuntime: at com.android.server.SystemServer.main(SystemServer.java:222)
01-01 00:00:28.974 511 511 E AndroidRuntime: at java.lang.reflect.Method.invoke(Native Method)
01-01 00:00:28.974 511 511 E AndroidRuntime: at com.android.internal.os.ZygoteInit$MethodAndArgsCaller.run(ZygoteInit.java:890)
01-01 00:00:28.974 511 511 E AndroidRuntime: at com.android.internal.os.ZygoteInit.main(ZygoteInit.java:780)
01-01 00:00:28.974 511 511 E AndroidRuntime: Caused by: java.lang.NullPointerException: Attempt to read from field 'int android.os.BatteryProperties.batteryLevel' on a null object reference
01-01 00:00:28.974 511 511 E AndroidRuntime: at com.android.server.BatteryService.processValuesLocked(BatteryService.java:331)
01-01 00:00:28.974 511 511 E AndroidRuntime: at com.android.server.BatteryService.updateBatteryWarningLevelLocked(BatteryService.java:237)
01-01 00:00:28.974 511 511 E AndroidRuntime: at com.android.server.BatteryService.onBootPhase(BatteryService.java:218)
01-01 00:00:28.974 511 511 E AndroidRuntime: at com.android.server.SystemServiceManager.startBootPhase(SystemServiceManager.java:143)
01-01 00:00:28.974 511 511 E AndroidRuntime: ... 8 more
01-01 00:00:28.988 511 511 I Process : Sending signal. PID: 511 SIG: 9I would love to know how to solve this. It already has taken me several days of debugging, and I don't know what to do next and I'm on the point of just removing code from the Android SDK in order to continue the boot.
this may help you.
Supporting Batteryless Devices | Android Open Source Project