AMP mode support for i.MX6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

AMP mode support for i.MX6

1,355件の閲覧回数
ramansubramania
Contributor I

It does not look like AMP mode is standard in all i.MX6 processors.  Is
that correct?

I don't see it in the datasheets or reference manuals, so
I am guessing that

most i.MX6's don't have AMP mode.  The confusion comes
because there are  websites which refer to the AMP ability with i.MX6
processors.

Can you please clear up this issue?

ラベル(1)
0 件の賞賛
返信
1 返信

1,025件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Raman

NXP supports i.MX6SX running linux + mqx, also please look at

MX6D example

https://community.freescale.com/docs/DOC-94513

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信