AMP boot ARM iMX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

AMP boot ARM iMX6

2,575 Views
lucatardioli
Contributor I

Hi all,

I'm working with an ARM Cortex A9 iMX6 with two CPUs and I would like to run two different O.S. (yocto, debian or other linux distribution in one core and freeRTOS in the other).

Actually I have downloaded the Uboot sources code from git repository

uboot-imx.git - Freescale i.MX u-boot Tree 

but I have very few experience in the Uboot programming and I like to have some advices about it.

I would like to run two O.S. without an Hypervisor but using uboot only. Is that possible?

Thanks in advice for help.

Labels (3)
Tags (2)
3 Replies

1,933 Views
dusancervenka-b
NXP Employee
NXP Employee

I am working on similar task.
I found only this http://www.dave.eu/sites/default/files/an-xelk-001-amp-linux-freertos.pdf  

0 Kudos
Reply

1,933 Views
wangzhimin
Contributor II

I also working with an ARM Cortex A9 iMX6 with two CPUs and I would like to run two different O.S. do you solve it

0 Kudos
Reply

1,933 Views
igorpadykov
NXP Employee
NXP Employee

Hi Luca

nxp does not support amp for i.MX6D/Q processors in its official bsps described on

i.MX 6 / i.MX 7 Series Software and Development Tool|NXP 

one can check third party solutions:

Boot The i.mx6 dual With Linux+uC/OS-II AMP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------