ALSA repeats and overlaps the sound with itself on all audio outputs - imx6 linux

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ALSA repeats and overlaps the sound with itself on all audio outputs - imx6 linux

ソリューションへジャンプ
1,318件の閲覧回数
atillametetured
Contributor V

Hello,

We have a custom i.MX6 board with S/PDIF and stereo outputs. When we run the speaker test;

speaker-test -t wav -c 1

The sound is repeated as if it is getting mixed with another instance of the same sound. What we hear is something like "front front left left" playing on top of each other instead of "front left" and no matter what we do with -c 1/2. We tried mingling with the configuration files and all and nothing seems to fix this problem. It is the same for both S/PDIF and the stereo outputs so it is not codec related.

Please someone advice what can be wrong.

Kind Regards,

Mete

ラベル(4)
0 件の賞賛
返信
1 解決策
1,205件の閲覧回数
atillametetured
Contributor V

This was fixed by decreasing the buffer_size in .asoundrc.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,206件の閲覧回数
atillametetured
Contributor V

This was fixed by decreasing the buffer_size in .asoundrc.

0 件の賞賛
返信