ALSA repeats and overlaps the sound with itself on all audio outputs - imx6 linux

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ALSA repeats and overlaps the sound with itself on all audio outputs - imx6 linux

Jump to solution
1,259 Views
atillametetured
Contributor V

Hello,

We have a custom i.MX6 board with S/PDIF and stereo outputs. When we run the speaker test;

speaker-test -t wav -c 1

The sound is repeated as if it is getting mixed with another instance of the same sound. What we hear is something like "front front left left" playing on top of each other instead of "front left" and no matter what we do with -c 1/2. We tried mingling with the configuration files and all and nothing seems to fix this problem. It is the same for both S/PDIF and the stereo outputs so it is not codec related.

Please someone advice what can be wrong.

Kind Regards,

Mete

Labels (4)
0 Kudos
Reply
1 Solution
1,146 Views
atillametetured
Contributor V

This was fixed by decreasing the buffer_size in .asoundrc.

View solution in original post

0 Kudos
Reply
1 Reply
1,147 Views
atillametetured
Contributor V

This was fixed by decreasing the buffer_size in .asoundrc.

0 Kudos
Reply