ALEXA NXP GIT access is blocked

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

ALEXA NXP GIT access is blocked

跳至解决方案
2,784 次查看
jorge2
Contributor I

Hi community,

We developed and manufactured custom i.MX8 board with Alexa running. We can't get it to work because there is an NXP git source that is blocked. 

This means we can't run the NXP solution that is supposed to run the NXP Alexa "out-of-the-box" solution.

Porting it from the pre-built image won't work as we also have a custom sound card.

We need the tar AWE_CL_8M.tar.bz2 to test out our i.MX8 board. How can we get access, or can you send it to us?

Thanks!

Jorge Reis

git.jpg

0 项奖励
回复
1 解答
2,645 次查看
diegoadrian
NXP Employee
NXP Employee

Hello,

Have you tried rebuilding the entire Alexa image but with this repo?

$ repo init -u https://source.codeaurora.org/external/imxsupport/meta-avs-demos -b master -m imx-alexa-sdk-4.9.51-8mq_ga.xml

 Apparently, the git that you are using is an old one.

Furthermore, the AWE_CL_8M.tar.bz2 is the package for the voice hat, that in your case, you are not using it. You will need to select "no" at the time you are running the Alexa SDK script and modify the following file. 

  • cp -v /etc/asound.conf /etc/asound.conf.BACKUP
  • cp -v /etc/asound.conf.Regular /etc/asound.conf

Otherwise, you will use the drivers from hardware that you do not have.

Hope this information could help you.

Best regards,

Diego.

在原帖中查看解决方案

2 回复数
2,646 次查看
diegoadrian
NXP Employee
NXP Employee

Hello,

Have you tried rebuilding the entire Alexa image but with this repo?

$ repo init -u https://source.codeaurora.org/external/imxsupport/meta-avs-demos -b master -m imx-alexa-sdk-4.9.51-8mq_ga.xml

 Apparently, the git that you are using is an old one.

Furthermore, the AWE_CL_8M.tar.bz2 is the package for the voice hat, that in your case, you are not using it. You will need to select "no" at the time you are running the Alexa SDK script and modify the following file. 

  • cp -v /etc/asound.conf /etc/asound.conf.BACKUP
  • cp -v /etc/asound.conf.Regular /etc/asound.conf

Otherwise, you will use the drivers from hardware that you do not have.

Hope this information could help you.

Best regards,

Diego.

2,645 次查看
jorge2
Contributor I

Thanks Diego. 

Yes, we are building with that repo.

Your hints about asound.conf were helpful. Our issue is sorted out.

Thanks!

JR

0 项奖励
回复