AIPSTZ in imx6.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

AIPSTZ in imx6.

3,128件の閲覧回数
myungjinhwang
Contributor III

Dear NXP team.

I have 2 questiosns...

1. AIPTZ

     There are AIPSTZ_PACRs, AIPSTZ_OPACRs registers as bellow in the reference menual(Document Number:      IMX6DQRM Rev. 3, 07/2015).

     but no descriptions of AIPSTZ_PACRs, it only explain AIPSTZ_OPACRs

     where can i find AIPSTZ_PACRs?

     13.6 Initialization Information

     The AIPS bridge should be programmed before use.

     The following registers should be initialized: The Master Privilege Registers

     (AIPSTZ_MPRs), the Peripheral Access Control registers (AIPSTZ_PACRs), and the

     Off-platform Peripheral Access Control registers (AIPSTZ_OPACRs) described in AIPSTZ Memory Map/Register      Definition.

2. AIPSTZx_MPR

     As bellow description, I need to control AIPSTZx_MPR register.

pastedImage_0.png

     and i could see something wonder.

     I think i could write only AIPSTZx_MPR(0x0207_C000) to control MOROT0, MOROT1, MOROT2, MOROT3

 

     But in the u-boot source code, it write 0x0207_C000 and 0x0207_C004 to control MOROT0, MOROT1 as bellow.

     It's different with the reference menual.

     then I should write 0x0207_C008,0x0207_C00C to control MOROT2, MOROT3?

     Please give some guide in detailed as possible.

/*
* Set all MPROTx to be non-bufferable, trusted for R/W,
* not forced to user-mode.
*/
writel(0x77777777, &aips1->mprot0);
writel(0x77777777, &aips1->mprot1);

     and the physical memory dump is that

________address|________0________4________8________C_0123456789ABCDEF

  AZSD:0207C000|>77777777 77777777 ???????? ???????? wwwwwwww????????

  AZSD:0207C010| ???????? ???????? ???????? ???????? ????????????????

Have a good day.

MyungJin Hwang

0 件の賞賛
返信
2 返答(返信)

2,538件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

1.

Below are definitions for registers offsets :

#define AIPS_MPROT0_7_OFFSET              0x00

#define AIPS_MPROT8_15_OFFSET              0x04

#define AIPS_PACR0_7_OFFSET              0x20

#define AIPS_PACR8_15_OFFSET              0x24

#define AIPS_PACR16_23_OFFSET              0x28

#define AIPS_PACR24_31_OFFSET              0x2C

#define AIPS_OPACR0_7_OFFSET              0x40

#define AIPS_OPACR8_15_OFFSET              0x44

#define AIPS_OPACR16_23_OFFSET              0x48

#define AIPS_OPACR24_31_OFFSET              0x4C

#define AIPS_OPACR32_33_OFFSET              0x50

The AIPS_PACR registers are skipped in the RM.

2.
  U-boot is based on preliminary i.MX6 specs, where master’s bit fields 4-15 (MPROT4-15)

were not declared as Reserved. Please follow the recent RM.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,538件の閲覧回数
myungjinhwang
Contributor III

Hi Yuri.

Thank you very much for the detailed answer.

It's very helpful.

Have a great day.

MyungJin

0 件の賞賛
返信