We use fsl-image-x11-imx6qdlsolo.sdcard from fsl-L3.10.17_1.0.2_iMX6QDLS_Bundle.tar.gz on MCIMX6Q-SDP. According to Xorg.0.log as below, AIGLX reverting to software rendering becuase /usr/lib/dri/vivante_dri.so has no __driDriverExtensions implementation. Where can we find the vivante_dri.so has driDriverExtensions implementation to has hardware rendering in X11?
[2370927.372] (EE) AIGLX error: vivante exports no extensions (/usr/lib/dri/vivante_dri.so: undefined symbol: __driDriverExtensions)
[2370927.372] (EE) AIGLX: reverting to software rendering
[2370927.563] (II) AIGLX: Loaded and initialized swrast
Original Attachment has been moved to: 20141217-mcimx6qsdp-x11-y3.10.17-1.0.2-Xorg.0.log-01.txt.zip
I would recommend looking at the following thread as this symptom seems to be normal and can be ignored. HW acceleration should work regardless
Hi all,
the reported link doesn't work any more.
Can you provide a new one?
Thanks,
Flavio
I'm having the same problem. Xorg reverts to software rendering. By the way, I have no access to this link. This is the message provided:
Access to this place or content is restricted. If you think this is a mistake, please contact your administrator or the person who directed you here
Any solution to this problem?