Hi,
I am trying to run Xorg server on imx6 SABRE-AI. I was able to build vivante
module using LTIB. I put it in the file system, and am
now able to load vivante_drv.so through display.conf settings.Just to confirm
everything is ok, pasting brief log:
[ 59.508]drmOpenDevice: node name is /dev/dri/card0
[ 59.509]drmOpenByBusid: Searching for BusID platform:Vivante GCCore
[ 59.509]drmOpenDevice: node name is /dev/dri/card0
[ 59.509]drmOpenDevice: open result is 11, (OK)
[ 59.509]drmOpenByBusid: drmOpenMinor returns 11
[ 59.509]drmOpenByBusid: Interface 1.4 failed, trying 1.1
[ 59.509]drmOpenByBusid: drmGetBusid reports platform:Vivante GCCore:00
Vivante driver loads a few more
modules (like fbdev,exa,fbdevhw etc), and I am getting some errors related to
AIGLX. Briefly, the message is something like this:
[ 59.514]drmOpenDevice: open result is -1, (No such device)
[ 59.514]drmOpenDevice: open result is -1, (No such device)
[ 59.514]drmOpenDevice: Open failed
[ 59.514]drmOpenByBusid: drmOpenMinor returns -19
[ 59.514] (EE) AIGLX error: drmOpenOnce failed(Operation not permitted)
[ 59.514] (EE) AIGLX: reverting to software rendering
[ 59.514] (II) AIGLX: Trying DRI driver /usr/lib/arm-linux-gnueabi/dri/swrast_dri.so
[ 59.646] (II)AIGLX: Loaded and initialized swrast
[ 59.646] (II)GLX: Initialized DRISWRAST GL provider for screen 0
[ 59.649] Fatal server error:
[ 59.649] Driver failed PrepareAccess on a pinned pixmap.
Xorg versions for various drivers are as follows:
(II) Module ABI versions:
[ 59.257] X.Org ANSI C Emulation: 0.4
[ 59.257] X.Org Video Driver: 10.0
[ 59.257] X.Org XInput driver : 12.3
[ 59.257] X.Org Server Extension : 5.0
I want to know whether it is a problem related to just X-org version or something else is going wrong !!attaching a detailed log generated by startx for reference.
Thanks and regards,
Prathamesh
Original Attachment has been moved to: display.conf.zip
Original Attachment has been moved to: Xorg.0.log.zip